Awards and Certifications
Standards We Meet. Honors We've Earned.
Our Awards
Our awards celebrate the people and projects that define IEM’s commitment to excellence.

#50 on Pacific Region List
Companies on the 2026 Inc. Regionals lists are ranked according to their percentage growth over two years, from 2022 to 2024. The honorees from the Pacific region added 7,503 jobs and $2.5 billion to the regional economy. IEM was listed #50 on Pacific Region list. For IEM this means lorem tempor sagittis dui quis tristique. Sed porttitor scelerisque nisi ac fringilla. Duis tincidunt lobortis varius.

#2 Largest Manufacturing Firm in Jacksonville
The largest manufacturing firms in the Jacksonville area employ more 1,800 workers on the First Coast. This online ranking expands beyond print, adding 10 manufacturing companies to the 15 featured in this week's print edition. IEM was listed as #2 Largest manufacturing companies.
For IEM this means lorem tempor sagittis dui quis tristique. Sed porttitor scelerisque nisi ac fringilla. Duis tincidunt lobortis varius.

Top 30 Largest Manufacturing Firm in the Bay Area
The largest manufacturing firms in the San Francisco Business Times and Silicon Valley Business Journal employ 72,202 local employees in the Greater Bay Area.
For IEM this meant lorem tempor sagittis dui quis tristique. Sed porttitor scelerisque nisi ac fringilla. Duis tincidunt lobortis varius.
Our Certifications
IEM’s products carry UL and CSA listings and are designed in accordance with applicable ANSI, IEEE, and NEMA standards.
Our quality management system is ISO 9001:2015 certified.

UL Listed
At IEM, we don’t believe in one-size-fits-all. From tailored switchgear and control systems to fully integrated power solutions, our portfolio is designed to meet the evolving needs of today’s most demanding environments.
Learn more about IEM's range of UL Listed switchgear, switchboards and panelboards. https://www.iemfg.com/products/

IEM Plants Certified ISO 9001
Bureau Veritas Certification Holding SAS certifies that the Management System of multiple IEM platns has been audited and found to be in accordance with the requirements of the management system standards .
For IEM this meant lorem tempor sagittis dui quis tristique. Sed porttitor scelerisque nisi ac fringilla. Duis tincidunt lobortis varius.

IEM Power Lab Certified Testing Facility
Industrial Electric Mfg. (IEM) has earned acceptance for its Power Lab in Tualatin, Oregon into CSA Group's Supervised Manufacturer's Testing for Certification (SMTC) program, a qualification that allows the company to conduct regulatory testing in-house and submit the results directly to CSA for certification, without a CSA engineer on-site.
The result is a shorter, more self-directed certification cycle that helps accelerate overall time-to-market for new or enhanced products requiring a CSA listing, a frequent need based on IEM’s portfolio of scalable custom configured power distribution equipment rather than fixed catalog models. By moving certification testing onto its own timeline, IEM removes an external hand-off from projects that previously had to wait for a witness to travel to the lab.
Products that carry a CSA Listing have generally required a certification representative to witness testing before the data can support a mark, a step that ties a manufacturer's schedule to the availability of an outside engineer. Under SMTC, that witness requirement is removed: a qualified facility generates its own test and evaluation data and provides it to CSA for third-party review and certification.
The achievement builds on the Power Lab's in-house testing and R&D capabilities, established when the facility opened in the Portland, Oregon, metro area in late 2024. Those capabilities include continuous current testing up to 6,000 A, lightning impulse testing up to 300 kV and dielectric withstand testing up to 200 kV, along with partial discharge testing to IEC 60270, mechanical endurance testing and environmental exposure testing for outdoor equipment.