News

News

LV Switchgear Distribution Now Rated to 200kA at 240V

Friday, November 14, 2008

VESTA-AR Datasheet  Download PDF

IEM, the largest independent full-line manufacturer of electrical and power quality equipment in the U.S., has added a panel with distribution certified to 200kA at 240V to its line of UL 891 low voltage switchgear.

“IEM has been building switchboard distribution “CDP” panels with a 100kA rating for a long time,” said Don Kozerski, Vice President of Marketing & Sales at IEM.  “We’ve now enhanced the panel design to meet UL test standards at 200kA, adding flexibility for customers that require distribution with high short circuit ratings.”

The new panel can be built in NEMA 1 or NEMA 3R enclosures.  It will be integral to the switchgear and can accommodate any input protective device rated 4kA or lower (circuit breaker or Class L fuse), easily coordinating with upstream breakers or fuses.

About IEM

Headquartered in Fremont, CA, IEM is the largest independent full-line manufacturer of electrical distribution and power quality equipment in the U.S.  For over half a century, IEM has delivered customer-specific solutions to meet the ever changing power requirements of growth industries in North America.  At IEM, tradition and technology still drive innovation.  An experienced engineering staff and one of the most flexible design and manufacturing systems in the industry set IEM apart from standard product manufacturers.